Hi,
The TWR-KV58F220M board 50MHz clock need resourcing from TWR-SER board, please disable the TWR-KV58F220M board 50MHz oscillator with J29 shunt on.
For the detailed clock setting for TWR-KV58F220M board, please check below info at [lwip_udpecho] project <readme.txt> file:
Board settings
==============
TWR-SER:
- RMII mode - J2 3-4 shunt on, J3 2-3 shunt on, J12 shunt on 9,10.
Clock setting for TWR-KV58F220M board
- J29 1-2 shunt on.
- Place R110 with 0 Ohm resister.
- J11 no shunt, to avoid wrong reset button behaviour.
BTW: The MCUXPresso SDK V2.3.1 for TWR-KV58F220M board [lwip_udpecho] project supported below IDE software:
Toolchain supported
===================
- IAR embedded Workbench 8.11.3
- Keil MDK 5.23
- GCC ARM Embedded 6-2017-q2
- Kinetis Development Studio IDE 3.2.0
- MCUXpresso10.1.0
The major issue is the TWR-KV58F220M board should use TWR-SER board 50MHz CLKIN.
Wish it helps.
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------