Why PTA4 LED in KL34 is ON by default and has 1v?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why PTA4 LED in KL34 is ON by default and has 1v?

836件の閲覧回数
abosamy
Contributor I

I use KL34 on my costume board. The problem is that once I connect it with power, the LED on PTA4 becomes ON. When I measured the voltage on it, It's 1v.

Why is this pin ON and why it's value is 1v?

ラベル(1)
0 件の賞賛
返信
1 返信

752件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Abo Samy,

    PTA4 is the NMI pin,  this is the input pin, not the output pin.

    If you want to use the GPIO to control the LED, please choose another pin, NMI is the Non maskable interrupt pin, you should add an 4.7K to 10K external pullup resistor in this pin.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信