Which pins support open drain output?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which pins support open drain output?

跳至解决方案
1,706 次查看
Laartoor
Contributor III

I am using the MK10DX256VLH7, and I want to use the open drain output functionality. When I check the data sheet, it tells me about the ODE bit in the PORTx_PCRn configuration register, and says in the features overview:

"Individual open drain field supporting enable and disable of the individual open drain output on selected pins"

Unfortunately I can nowhere find a list telling me which pins support open drain output. Does this exist anywhere?

( I could test every pin by checking whether I can change ODE, but I would rather not go that route)

0 项奖励
回复
1 解答
1,564 次查看
santiago_lopez
NXP Employee
NXP Employee

Hi Laartoor,

The MCU you are using supports ODE on all its GPIOs so you don´t have to worry. Other MCUs like the Kinetis KL26 have restrictions in certain pins. In this specific case, you can find those restrictions in the MCU Reference Manual on the Chapter 3 "Chip Configuration" under the section "Human-machine interfaces-->GPIO configuration"

Saludos

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,564 次查看
Laartoor
Contributor III

Gracias

0 项奖励
回复
1,565 次查看
santiago_lopez
NXP Employee
NXP Employee

Hi Laartoor,

The MCU you are using supports ODE on all its GPIOs so you don´t have to worry. Other MCUs like the Kinetis KL26 have restrictions in certain pins. In this specific case, you can find those restrictions in the MCU Reference Manual on the Chapter 3 "Chip Configuration" under the section "Human-machine interfaces-->GPIO configuration"

Saludos

0 项奖励
回复