Which is valid, upper or lower of CRC_CRC in 16-bit CRC mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which is valid, upper or lower of CRC_CRC in 16-bit CRC mode?

Jump to solution
2,172 Views
yasuhikokoumoto
Senior Contributor I

Hello experts,

I have a question of the crc_demo sample in KINETIS_120MHZ_SC provided by the freescale.

According to Kinetis K70 Reference Manual "35.3.2.1 16-bit CRC", the usage of CRC_CRC is described as below.

6. Clear the CTRL[WAS] bit to start writing data values.
7. Write data values into CRC[HU:HL:LU:LL]. A CRC is computed on every data
value write, and the intermediate CRC result is stored back into CRC[LU:LL].
8. When all values have been written, read the final CRC result from CRC[LU:LL].


I think it would be inconsistent with the sample code.

The original code is as follows.

  sizeWords = sizeBytes>>1;   j = 0;   for(i=0;i<sizeWords;i++){       data_in = (msg[j] << 8) | (msg[j+1]);       j += 2;       CRC_CRCH=data_in;                 //DES was CRC_CRC_LOW=data_in;   }   if(j<sizeBytes)   {      pCRCBytes = (uint8_t*)&CRC_CRC;      *pCRCBytes++ = msg[j];   }   data_out=CRC_CRCH;                    //DES was CRC_CRC;

I guess it might be as follows.

  sizeWords = sizeBytes>>1;   j = 0;   for(i=0;i<sizeWords;i++){       data_in = (msg[j+1] << 8) | (msg[j]); // CHANGE       j += 2;       CRC_CRCL=data_in;                    // CHANGE   }   if(j<sizeBytes)   {      pCRCBytes = (uint8_t*)&CRC_CRC;      *pCRCBytes++ = msg[j];   }   data_out=CRC_CRCL;                        //CHANGE


Am I not correct?

Can anyone teach me the truth?

Best regards,

Yasuhiko Koumoto.

Tags (3)
0 Kudos
Reply
1 Solution
1,780 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Yasuhiko Koumoto:

I think the sample code is correct and your confusion is about endianness. In the sample project, the message buffer is filled from a UART channel in sequence, so you can consider that the bytes are stored in Big Endian mode:

printf("\r\nPlease enter an ASCII Message:");

bByteCount = Input_Message(&strMsg[0]);

...

uint32_t  Input_Message(uint8_t *MsgBuf)

{

  uint8_t ch;

  uint32_t count;

 

  count = 0;

  do

  {

    ch = in_char();

    out_char(ch);

    if(ch == '\r')

    {    

      break;

    }

    MsgBuf[count++] = ch;

    if(count >= MAX_CHARS)

    {

      break;

    }

  }while(1);

   

  return (count);

}

But the CRC registers in K70 are Little Endian, so the correct way to calculate CRC16 for this buffer is with the original code:

sizeWords = sizeBytes>>1;

  j = 0;

  for(i=0;i<sizeWords;i++){

      data_in = (msg[j] << 8) | (msg[j+1]);

      j += 2;

      CRC_CRCL=data_in;

  }

  if(j<sizeBytes)

  {

     pCRCBytes = (uint8_t*)&CRC_CRC;

     *pCRCBytes++ = msg[j];

  }

  data_out=CRC_CRC;  // CRC_CRCL is also correct

return(data_out);


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
1,780 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Koumoto-san

Please pay more patience. I will check your issue. Thanks.

Best Regards

Paul

0 Kudos
Reply
1,780 Views
yasuhikokoumoto
Senior Contributor I

Hi Paul,

thank you. I am interested in the result.

Best regards,
Yasuhiko Koumoto.

0 Kudos
Reply
1,780 Views
PatriciaTeran
Contributor III

Hi, Yasuhiko

Are you still having problems?

Regards

Patricia

0 Kudos
Reply
1,780 Views
yasuhikokoumoto
Senior Contributor I

Hello Patricia,

I have still problem because I have not gotten any answer from Paul.

Best regards,

Yasuhiko Koumoto.

0 Kudos
Reply
1,781 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Yasuhiko Koumoto:

I think the sample code is correct and your confusion is about endianness. In the sample project, the message buffer is filled from a UART channel in sequence, so you can consider that the bytes are stored in Big Endian mode:

printf("\r\nPlease enter an ASCII Message:");

bByteCount = Input_Message(&strMsg[0]);

...

uint32_t  Input_Message(uint8_t *MsgBuf)

{

  uint8_t ch;

  uint32_t count;

 

  count = 0;

  do

  {

    ch = in_char();

    out_char(ch);

    if(ch == '\r')

    {    

      break;

    }

    MsgBuf[count++] = ch;

    if(count >= MAX_CHARS)

    {

      break;

    }

  }while(1);

   

  return (count);

}

But the CRC registers in K70 are Little Endian, so the correct way to calculate CRC16 for this buffer is with the original code:

sizeWords = sizeBytes>>1;

  j = 0;

  for(i=0;i<sizeWords;i++){

      data_in = (msg[j] << 8) | (msg[j+1]);

      j += 2;

      CRC_CRCL=data_in;

  }

  if(j<sizeBytes)

  {

     pCRCBytes = (uint8_t*)&CRC_CRC;

     *pCRCBytes++ = msg[j];

  }

  data_out=CRC_CRC;  // CRC_CRCL is also correct

return(data_out);


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply