Which are the options for programming a MKW41Z custom board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which are the options for programming a MKW41Z custom board?

跳至解决方案
1,332 次查看
javiermonrealtr
Contributor II

Good evening,

I tested the FRDM-KW41Z evaluation board and I've decided to design a custom board with the MKW41Z MCU as its core. But what options do I have for programming it, and which do you recommend?

I know two: Using the U-MULTILINK tool (https://www.digikey.es/product-detail/es/nxp-usa-inc/U-MULTILINK/U-MULTILINK-ND/2660579) or using an FRDM-KW41Z as a programmer (https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/)

I will build three units of the custom board device, so I'm looking for the easiest although not most efficient programming option.

Thanks in advance!

1 解答
1,199 次查看
BlackNight
NXP Employee
NXP Employee

You have more options, for example:

- Segger J-Link (J-Link Debug Probes | SEGGER - The Embedded Experts ), e.g. for non-commercial the J-Link EDU (starts at around 20 Euro) which are available from distributors too

- If you are using the MCUXpresso IDE, there is the LPC-Link2 (around 20 Euro too), see Custom 3D Printed Enclosure for NXP LPC-Link2 Debug Probes | MCU on Eclipse 

I hope this helps,

Erich

在原帖中查看解决方案

1 回复
1,200 次查看
BlackNight
NXP Employee
NXP Employee

You have more options, for example:

- Segger J-Link (J-Link Debug Probes | SEGGER - The Embedded Experts ), e.g. for non-commercial the J-Link EDU (starts at around 20 Euro) which are available from distributors too

- If you are using the MCUXpresso IDE, there is the LPC-Link2 (around 20 Euro too), see Custom 3D Printed Enclosure for NXP LPC-Link2 Debug Probes | MCU on Eclipse 

I hope this helps,

Erich