Which MCU is best for my purpose

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which MCU is best for my purpose

1,823 Views
ioniriondo
Contributor I

Hi.

I'm looking for an MCU which fits my purpose, and I would appreciate if you could help me with this.

I've been working with the Kinetis K60 for some applications, but now I need a much simplier one.

What I need is just Analog Input/Output (this could be done via I2C, etc...) and Can Bus communication.

Also, as smaller, better.

Thanks.

Tags (2)
0 Kudos
Reply
4 Replies

1,639 Views
LuisCasado
NXP Employee
NXP Employee

Hi Ion,

The MK10DX64VLH7 is the snallest Kinetis K (Cortex M4)  with CAN. With your experience in K60, K10 will be easy to use.

Other option would be KE06 (Cortex M0+)  at 5V that will be launched very soon.


Regards,

Luis

1,639 Views
ioniriondo
Contributor I

Hi Luis.

I had taken a look to that model too. As you say, I think would be much easier to work with it as I have previously worked with another Kinetis model. Anyway, I still have to take a look if the size of this fits our purpose.

About the KE06, when will be it lanched more or less? At a first look, I've seen that is kind a evolution of the S08 MCU. Again, I will have to think what to choose between a fast programming but with a larger size, and a smaller one but with I would have to spend more time in programming.

0 Kudos
Reply

1,639 Views
Robinwithu
Senior Contributor I

Hi Ion,

Here is few 8 bit controller with CAN BUS n  Analog input.

MC9S08DZ60

MC9S08DZ48

MC9S08DZ32

MC9S08DZ16

Thanks n Regards,

Robin

1,639 Views
ioniriondo
Contributor I

Is there any example code to start working with those models? The size is perfect for my aplication, but I think using a Kinetis model would be faster due to as Luis Casado has said, I've worked with it and I have part of code (Initializations, desing,  etc...) that I can use. So, I wouldn't have to spend much time at starting.

0 Kudos
Reply