Which IDE should I use for FRDM-KE16Z64VLD4 MCU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which IDE should I use for FRDM-KE16Z64VLD4 MCU?

跳至解决方案
2,882 次查看
whiteliondd6
Contributor I

I am trying to configure the pins of  FRDM-KE16Z64VLD4 using MCUXpresso v11.5.0. But, it is showing me the waring "Board configuration files are not designed and might not work with the selected device." Also, after generating the project when I tried to use config tools it was not opening. So, is there any installation error or I should use other IDE. Suggest me how to fix the errors or which IDE should I use?

 

0 项奖励
回复
1 解答
2,780 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello whiteliondd6

I was facing your issue and I think have this might help you.

The MCU config tool read the files in de folder "board" and the pop-up Error shows the no coincidence with the board.

I found this is an error for peripherals.c, please open this and change the MKE15Z256xxx7 to MKE16Z256xxx7 like the image show and make a compile and try to open again the "Config pin".

Pavel_Hernandez_1-1645210280733.png

Regards

Pavel_Hernandez

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,833 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello whiteliondd6

I’m still review your case; please could you upload the image of your error please so we can check the root of your issue.

Could you please try to select the board instead of selecting the part number of the uC ?

Regards,
Pavel_Hernandez

0 项奖励
回复
2,812 次查看
whiteliondd6
Contributor I

I tried for both i.e. directly selected the uC part number and then I selected board both the result is same.

Here, I am sharing the error shanpshot.

thumbnail_Capture.png

0 项奖励
回复
2,862 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello whiteliondd6

I'm here to help you in your case. But first I need more information about your environment, please could you give me the version of your SDK.

Or I suggest to download a new SDK and I recommend you select the MCUXpresso IDE toolchain.

MicrosoftTeams-image.png

Best regards

Pavel_Hernandez

0 项奖励
回复
2,858 次查看
whiteliondd6
Contributor I

Capture.PNG

 I am using SDK version 2.11.0 with mcuxpresso toolchain.  Still, facing the issue.

 

0 项奖励
回复
2,781 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello whiteliondd6

I was facing your issue and I think have this might help you.

The MCU config tool read the files in de folder "board" and the pop-up Error shows the no coincidence with the board.

I found this is an error for peripherals.c, please open this and change the MKE15Z256xxx7 to MKE16Z256xxx7 like the image show and make a compile and try to open again the "Config pin".

Pavel_Hernandez_1-1645210280733.png

Regards

Pavel_Hernandez

0 项奖励
回复