I have my TWR-K24F120M board in bootloader mode, there are no useful files on it, the htm is a broken link to mbed.org. Where is the openSDA file for the K24 that I need to download to be able to debug from KDS?
Thanks,
Ian
解決済! 解決策の投稿を見る。
Hi Ian,
This is a board with OpenSDA v2.1 firmware on it.
You can debug it either with a P&E or Segger (Segger J-Link Firmware for OpenSDAv2 | MCU on Eclipse) connection (instructions shown for FRDM-K64F, but very similar for the TWR-K24F120M).
The Segger firmware is available from SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2: make sure you use the V2.1 firmware!
For P&E, if you are using Kinetis Design Studio V2.0.0, then the P&E OpenSDA firmware file is in
C:\Freescale\KDS_2.0.0\pemicro\opensda\DEBUG-TWR-K24F120M_Pemicro_v108b_for_OpenSDA_v2.1.bin
I recommend to upgrade to v2.0.0 (see Kinetis Design Studio V2.0.0 available on the Web!).
Otherwise you can download the firmware files (Firmware Aps) from the P&E website (P&E Microcomputer Systems).
See as well OpenSDAv2
I hope this helps,
Erich
Hi Ian,
This is a board with OpenSDA v2.1 firmware on it.
You can debug it either with a P&E or Segger (Segger J-Link Firmware for OpenSDAv2 | MCU on Eclipse) connection (instructions shown for FRDM-K64F, but very similar for the TWR-K24F120M).
The Segger firmware is available from SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2: make sure you use the V2.1 firmware!
For P&E, if you are using Kinetis Design Studio V2.0.0, then the P&E OpenSDA firmware file is in
C:\Freescale\KDS_2.0.0\pemicro\opensda\DEBUG-TWR-K24F120M_Pemicro_v108b_for_OpenSDA_v2.1.bin
I recommend to upgrade to v2.0.0 (see Kinetis Design Studio V2.0.0 available on the Web!).
Otherwise you can download the firmware files (Firmware Aps) from the P&E website (P&E Microcomputer Systems).
See as well OpenSDAv2
I hope this helps,
Erich
Is there a bootloader for the TWR-K24F120M that supports drag and drop programming? The "Getting Started with Kinetis TWRK24F120M" document states the following:
"At the time of writing this document there are two OpenSDAv2.1 applications that support the TWR-K24F120M:
• OpenLINK for TWR-K24F120M - Programmed on the board by default. Application download available at
freescale.com/TWR-K24F120M
• Segger JLink - Needs to be programmed into the OpenSDAv2 circuit to use Kinetis Design Studio projects.
Application available at segger.com/opensda.html (firmware links are at the bottom of the page)"
From your previous post I tried the segger and P&E bootloaders, but neither appears to support drag and drop programming. Where can I find the OpenLINK bootloader (I don't see it at freescale.com/TWR-K24F120M)?
Thanks for any help!