Where do I get new versions of MKL25Z4.h?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where do I get new versions of MKL25Z4.h?

ソリューションへジャンプ
2,826件の閲覧回数
markosiponen
Contributor III

I'm testing some code on the FRDM-KL25Z board. And I have tried the processor expert and then the Keil µVision. I noticed that Keil has an old MKL25Z4.h file.

The processor expert generates an IO_Map.h file that really is the MKL25Z4.h file. But the file that PE generates is a newer version than in Keil.

Where do I get new versions of these files for Kinetis MCUs (exept getting them from PE)?

0 件の賞賛
返信
1 解決策
1,909件の閲覧回数
chris_brown
NXP Employee
NXP Employee

Hi Markosiponen,

You could get them from the KL25_SC repository available at www.freescale.com/frdm-kl25z/.

~Chris

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,909件の閲覧回数
JimDon
Senior Contributor III

It is in the Codewarrior directories.

To find it, generate a non PE projects, the open it in the IDE and see where it is.

0 件の賞賛
返信
1,909件の閲覧回数
markosiponen
Contributor III

But what if I don't have Codewarrior?

0 件の賞賛
返信
1,910件の閲覧回数
chris_brown
NXP Employee
NXP Employee

Hi Markosiponen,

You could get them from the KL25_SC repository available at www.freescale.com/frdm-kl25z/.

~Chris

0 件の賞賛
返信
1,909件の閲覧回数
markosiponen
Contributor III

Where can I find similar files for other freescale MCUs?

0 件の賞賛
返信