Where can I find the demo source code of KL02Z?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find the demo source code of KL02Z?

ソリューションへジャンプ
4,141件の閲覧回数
jinbuhm_kim
Contributor II

Hi,

I found the FRDM-KL02-LAB GUIDE file as attached.

Where can I find the demo source code?

For example,  Demo 1: KL02_Freedom_Demo? 

Thanks,

JB#

ラベル(1)
タグ(4)
1 解決策
3,927件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello JIN BUHM KIM,

You can download the demo source code from the following link.

If you are looking for demos and drivers with their source code for the FRDM-KL02Z I highly recommend you download the SDK instead. SDK is a collection of comprehensive software enablement for NXP® Kinetis Microcontrollers that includes system startup, peripheral drivers, USB and connectivity stacks, middleware, and real-time operating system (RTOS) kernels. Link to download the newest version of the SDK. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

元の投稿で解決策を見る

6 返答(返信)
3,927件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Reference binary for FRDM-KL02Z with dynamic low power operation: http://www.utasker.com/kinetis/FRDM-KL02Z.html and KL02 simulation.
Free open source on Github and works with Codewarrior, KDS, MCUXpresso, IAR, Keil, Green Hills, Rowley Crossworks, Atollic, CooCox and Visual Studio.

See also this video of a KL02 (with small I2C slave loader installed) being updated by a FRDM-K64F board acting as master, carrying an image of the slave's application firmware: https://youtu.be/awREsqeCEzQ

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html
Kinetis KL02/KL03/KL05:
- http://www.utasker.com/kinetis/FRDM-KL02Z.html
- http://www.utasker.com/kinetis/FRDM-KL03Z.html
- http://www.utasker.com/kinetis/FRDM-KL05Z.html

For less questions and faster, cheaper developments: try uTasker for Kinetis

3,927件の閲覧回数
jinbuhm_kim
Contributor II

Hi Mark,

Thanks for the information.

JB

0 件の賞賛
返信
3,928件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello JIN BUHM KIM,

You can download the demo source code from the following link.

If you are looking for demos and drivers with their source code for the FRDM-KL02Z I highly recommend you download the SDK instead. SDK is a collection of comprehensive software enablement for NXP® Kinetis Microcontrollers that includes system startup, peripheral drivers, USB and connectivity stacks, middleware, and real-time operating system (RTOS) kernels. Link to download the newest version of the SDK. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

3,927件の閲覧回数
jinbuhm_kim
Contributor II

Hello Victor,

The demo source code is based on CW, IAR and KEIL.

Do you have demo code for MCUXpresso? 

If so, it'll be really helpful to me.

Thanks,

JB

0 件の賞賛
返信
3,927件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello JB,

The FRDM-KL02-LAB GUIDE was before the SDK. When the SDK appeared these projects stopped receiving updates, this is why the source code was never migrated to MCUXpresso.   

Regards,

Victor. 

0 件の賞賛
返信
3,927件の閲覧回数
jinbuhm_kim
Contributor II

Hi, Victor

I already download the SDK but couldn't find the demo code.

Thanks for your help. :smileyhappy:

0 件の賞賛
返信