Where can I find the bootloader image (elf) for TWR-K24F120M?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find the bootloader image (elf) for TWR-K24F120M?

ソリューションへジャンプ
1,324件の閲覧回数
javiercardona
Contributor III

I mistakenly connected my debugger to the wrong SWD connector and wiped the image on the K20 (SDA) microcontroller.  :smileycry:

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,177件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Javier,

    The MBED opensda v2.1 can be download from this link:

https://developer.mbed.org/media/uploads/GregC/k20dx128_bootloader_v21_0x8000.bin

 

Wish it helps you!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,178件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Javier,

    The MBED opensda v2.1 can be download from this link:

https://developer.mbed.org/media/uploads/GregC/k20dx128_bootloader_v21_0x8000.bin

 

Wish it helps you!

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,177件の閲覧回数
mjbcswitzerland
Specialist V

Hi Javier

Usually one can find the bootloaders at the P&E web site.

I have attached the one that I have for this board.

Regards

Mark

0 件の賞賛
返信