Where can I find specifications on the DMA maximum rate for the KL26 sub familiy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find specifications on the DMA maximum rate for the KL26 sub familiy

854 Views
alejandra25
Contributor I

I am trying to find out the maximum DMA rate for the  KL26 sub familiy (in particular for  the MKL26Z128).

I see that for other devices there is a section in the chapter of eDMA in the reference manual that specifies it. Here is an example on the K60 Sub-Family Reference Manual:

pastedImage_6.png

Where can i find this specifications for the  KL26 sub familiy microcontroller runnig at 480MHz ? The reference manual does not seem to have a -Performance- section.

Thank you very much.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

741 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I will check with Kinetis team about related DMA module performance data.

Thank you for the patience.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply