Where are MKL27Z4_registers.h/_features.h files found?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where are MKL27Z4_registers.h/_features.h files found?

1,132 Views
bobpaddock
Senior Contributor III

Where do I find these files:

    #define KL27Z4_SERIES

    /* CMSIS-style register definitions */

    #include "device/MKL27Z4/MKL27Z4.h"

    /* Extension register definitions */

    #include "device/MKL27Z4/MKL27Z4_registers.h"

    /* CPU specific feature definitions */

    #include "device/MKL27Z4/MKL27Z4_features.h"

they are referenced in fsl_devices_registers.h

Not finding them in KDS 3.2.0 tree nor the KSDK 2.0 built for the KL27  built by the online builder (it only has the MKL27Z644).

0 Kudos
Reply
3 Replies

891 Views
bobpaddock
Senior Contributor III

The part I'm using is the KL27Z256LK4.

Where are the header files I asked about?
Are you saying the MKL27Z644 headers have replaced the MKL27Z4 headers?

This is what MKL27Z4.h files says at the top:

Pre CMSIS:

** ###################################################################

**     Processors:          MKL27Z256VFM4

**                          MKL27Z128VFM4

**

**     Compilers:           ARM Compiler

**                          Freescale C/C++ for Embedded ARM

**                          GNU C Compiler

**                          IAR ANSI C/C++ Compiler for ARM

**

**     Reference manual:    KL27PxxM48SF4RM, Rev.1, May 2014

**     Version:             rev. 1.1, 2014-05-26

**     Build:               b140528

Newer CMSIS version (which requires the missing headers that I asked about.  Find it frustrating we are wasting time rather than just answering the question that was asked.  Where is MKL27Z4_registers.h?).

**     Processors:  MKL27Z256VFM4

**                          MKL27Z128VFM4

**                          MKL27Z256VFT4

**                          MKL27Z128VFT4

**                          MKL27Z256VLH4

**                          MKL27Z128VLH4

**                          MKL27Z256VMP4

**                          MKL27Z128VMP4

**

**     Compilers:           Keil ARM C/C++ Compiler

**                          Freescale C/C++ for Embedded ARM

**                          GNU C Compiler

**                          GNU C Compiler - CodeSourcery Sourcery G++

**                          IAR ANSI C/C++ Compiler for ARM

**

**     Reference manual:    KL27P64M48SF6RM, Rev.3, Aug 2014

**     Version:             rev. 1.6, 2015-02-12

**     Build:               b150212

0 Kudos
Reply

891 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello BOB,

when create project on KDS, select the chip of MKL27Z256, there will be the header files about this chip.

pastedImage_0.png

pastedImage_1.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

891 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bob,

Please check the part number of your chip ,

on the KDS+KSDK, for the different chip there is the corresponding header file  :

MKL27Z644.h  MKL27Z1284.h  ....

So please be sure your chip .

Hope it helps

Alice


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply