Hello @hangyoKim, Good Day!
Thank you for your interest in our products.
I would like to ask if you could please provide more details about the process followed up to this point. Could you please specify what are the settings or modifications that you have made for connecting the PNEV5190 to an external host?
I would like to ask as well, what are you trying to achieve with your setup and how are you testing it?
Please confirm, what is the firmware you are trying to flash? On which IC are you trying to flash it? And what are the steps you have taken in order to do so? Are you using the MCUXpresso IDE?
When you say the clock is not coming out from the crystal, do you mean the SPI clock? If not, how are you testing this? Note that the SPI clock must be generated by the host MCU and not by the PN5190.
Please consider that connecting the PNEV5190 via USB using the j20 port is only necessary when using the OpenSDA interface to flash the onboard k82.
Consider as well that in order to connect an external host via the SPI interface some hardware modifications have to be made to the board, please refer to section 2 of the PN5190 EMV L1 SW porting to IMX1170 app note in which you will find related details that you can use as a starting point when using the MCXN947 host MCU.
My best regards,
Daniel