When is SR[STF] flag set in DryIce in K81 MCU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When is SR[STF] flag set in DryIce in K81 MCU?

1,049 次查看
ste
Contributor I

K81 MCU in DryIce has a SR(Status Register).

SR Bit 7 (Security Tamper Flag) is set "when the (optional) security module asserts its tamper detect" according to the K81 User Manual.

Further:

"The SR[STF] bitfield description refers to an "(optional) security module". The 2KB
secure SRAM is the security module integrated into this device."

and according to a note in the UM: "A system reset causes STF to be set because the secure SRAM
detects a system reset as a tamper event."

Could anybody explain about the circumstances this flag is really set.

So far I've been working with K81 and monitoring various tamper flags but never managed to create a condition that would set STF.

Is it really active and linked to secure SRAM in the K81 MCUs ?

标签 (1)
0 项奖励
回复
1 回复

928 次查看
miduo
NXP Employee
NXP Employee

Hello,

Well, more detailed information for K81 DryIce Tamper Detect issue is under NDA. We will not discuss/disclose it within community. You may put a ticket here:Support|NXP and provide the NDA number then we can give more detail information. Thanks for your consideration.

0 项奖励
回复