What's the correct way to setup an IN and OUT endpoint in the USB_App_Class_Callback?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the correct way to setup an IN and OUT endpoint in the USB_App_Class_Callback?

649件の閲覧回数
brendanmerna
Contributor IV

I'm trying to add an OUT endpoint to the keyboard example project. I can't seem to get it to detect the USB_DEV_EVENT_DATA_RECEIVED. I'm writing 1 byte of USB data from Perisoft's Bus Hound application. Then endpoints are detected by it, but when I do a write the flag USB_DEV_EVENT_DATA_RECIEVED is never set. Is this the correct way to detect reads? What else should I do?


/******************************************************************************
*
* @name USB_App_Class_Callback
*
* @brief This function handles USB-HID Class callback
*
* @param request : request type
* @param value : give report type and id
* @param data : pointer to the data
* @param size : size of the transfer
*
* @return status
* USB_OK : if successful
* else return error
*
*****************************************************************************
* This function is called whenever a HID class request is received. This
* function handles these class requests.
*****************************************************************************/
uint8_t USB_App_Class_Callback(uint8_t request, uint16_t value, uint8_t ** data, uint32_t* size, void* arg)
{
   uint8_t error = USB_OK;
   uint8_t index = (uint8_t)((request - 2) & USB_HID_REQUEST_TYPE_MASK);


   if ((request == USB_DEV_EVENT_SEND_COMPLETE) && (value == USB_REQ_VAL_INVALID))
   {

      if ((g_keyboard.keyboard_init) && (arg != NULL))
      {
         KeyBoard_Events_Process(); /* run the cursor movement code */
      }

      return error;

   }

   if ((request == USB_DEV_EVENT_DATA_RECEIVED) && (value == USB_REQ_VAL_INVALID))
   {
      if((g_keyboard.keyboard_init) && (arg != NULL))
      {
         KeyBoard_Events_Set();
      }
      return error;
   }
   /* index == 0 for get/set idle, index == 1 for get/set protocol */
   /* handle the class request */
   switch(request)
   {
      case USB_HID_GET_REPORT_REQUEST:
         *data = &g_keyboard.rpt_buf[0]; /* point to the report to send */
         *size = KEYBOARD_BUFF_SIZE; /* report size */
         break;
      case USB_HID_SET_REPORT_REQUEST:
         for (index = 0; index < (*size); index++)
         {
            /* copy the report sent by the host */
            //g_keyboard.rpt_buf[index] = *(*data + index);
         }
         *size = 0;
         break;
   case USB_HID_GET_IDLE_REQUEST:
      /* point to the current idle rate */
      *data = &g_keyboard.app_request_params[index];
      *size = REQ_DATA_SIZE;
      break;
   case USB_HID_SET_IDLE_REQUEST:
      /* set the idle rate sent by the host */
      g_keyboard.app_request_params[index] = (uint8_t)((value & MSB_MASK) >> HIGH_BYTE_SHIFT);
      *size = 0;
      break;
   case USB_HID_GET_PROTOCOL_REQUEST:
      /* point to the current protocol code
      0 = Boot Protocol
      1 = Report Protocol*/
      *data = &g_keyboard.app_request_params[index];
      *size = REQ_DATA_SIZE;
      break;
   case USB_HID_SET_PROTOCOL_REQUEST:
      /* set the protocol sent by the host
      0 = Boot Protocol
      1 = Report Protocol*/
      g_keyboard.app_request_params[index] = (uint8_t)(value);
      *size = 0;
      break;
   }
   return error;
}

ラベル(1)
0 件の賞賛
返信
0 返答(返信)