What means TWR-KV58F220M with TWR-MC-LV3PH AUX signal?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What means TWR-KV58F220M with TWR-MC-LV3PH AUX signal?

471 Views
ristomustonen
Contributor II

Hello, I am using TWR-KV58F220M with TWR-MC-LV3PH board and motor control package MCRSP_PMSM_V1.2.0. I am checking out  the ADC connections for the motor control. I have found the following measurement channels:

M1_ADC0_PH_A (2)
M1_ADC1_PH_A (2)
M1_ADC1_PH_B (3)
M1_ADC0_PH_C (7)
M1_ADC0_UDCB (6)
M1_ADC1_AUX (6)

I am wondering what is the AUX signal, because I haven't found any explanation about it.

It would be great, if anyone can help me with this question.

BR, Risto

0 Kudos
2 Replies

342 Views
ristomustonen
Contributor II

Thank you, Robin. This is a good AN for the MC package.

0 Kudos

342 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Risto,

Please refer below information descripted in AN5237.

M1_ADC[0,1]_AUX.jpg

 

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos