Hello, I am using TWR-KV58F220M with TWR-MC-LV3PH board and motor control package MCRSP_PMSM_V1.2.0. I am checking out the ADC connections for the motor control. I have found the following measurement channels:
M1_ADC0_PH_A (2)
M1_ADC1_PH_A (2)
M1_ADC1_PH_B (3)
M1_ADC0_PH_C (7)
M1_ADC0_UDCB (6)
M1_ADC1_AUX (6)
I am wondering what is the AUX signal, because I haven't found any explanation about it.
It would be great, if anyone can help me with this question.
BR, Risto
Thank you, Robin. This is a good AN for the MC package.
Hi Risto,
Please refer below information descripted in AN5237.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------