What is the reason for Green Light Blinking in TRK-KEA-128 Development board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the reason for Green Light Blinking in TRK-KEA-128 Development board?

1,007件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    I was working on KEA-128 Bootloader and after some time saw that the Green light was blinkiing on the TRK-KEA-128 Develpment board and I was not able to flash new code.I don't know what is the reason behind it and How to fix it?

ラベル(2)
タグ(1)
1 返信

869件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Vignesh,

is this the green OpenSDA LED? If it blinks, then it is either in bootloader mode or blinks an error code.

In both cases it means you cannot debug it because there is no debug application.

Are you using Windows 10? In that case there is a known problem where Windows 10 can erase the debug application or even the bootloader itself. See https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/ . The article includes a table of error codes too.

I hope this helps,

Erich