What is the meaning of the Errata e7166?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the meaning of the Errata e7166?

跳至解决方案
1,518 次查看
yasuhikokoumoto
Senior Contributor I

Hi Freescale peoples,

I would like to know the meaning of the errata e7166. The background is that USB, NFC and SDHC are in static state or OFF state at STOP, VLPS, LLS and VLLSx modes. So I think it is a reasonable restriction to ensure no outstanding transaction on the bus-matrix. Therefore, I don't know what the errata e7166 want to make caution. Can you explain why the errata exists? Is it applied only to VLPW mode?

I have another question. In the errata, the target devices are limited to Kinetis K series. Why is the errata not applied to Kinetis L series? By simple thinking, the clock supply to the bus-matrix stops after each module of Kinetis L.  In this condition, why can Kinetis L survive even in the low power modes?

Best regards,
Yasuhiko Koumoto.

标记 (3)
0 项奖励
回复
1 解答
1,282 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check Kinetis K series product reference manual, such as K70 reference manual Table 7-2. Module operation in low power modes, which shows NFC and SDHC is full function at VLPW mode.

The errata e7166 shows below multiplexer is clock shut off when entry into any low power mode. From the application consideration, this errata only be available for VLPW low power mode.

crossbar.png

The Kinetis L series product is using Crossbar-light switch, which without the multiplexer. That's why this errata info not be suitable to Kinetis L series product.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,283 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check Kinetis K series product reference manual, such as K70 reference manual Table 7-2. Module operation in low power modes, which shows NFC and SDHC is full function at VLPW mode.

The errata e7166 shows below multiplexer is clock shut off when entry into any low power mode. From the application consideration, this errata only be available for VLPW low power mode.

crossbar.png

The Kinetis L series product is using Crossbar-light switch, which without the multiplexer. That's why this errata info not be suitable to Kinetis L series product.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,282 次查看
yasuhikokoumoto
Senior Contributor I

Hi Ma Hui,

thank you! I understood well.

Best regards,

Yasuhiko Koumoto.

0 项奖励
回复