What is the function of "TOWER ELEVATOR"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the function of "TOWER ELEVATOR"?

Jump to solution
1,575 Views
qzy_perfect
Contributor III

Hello everyone,

     What is the function of TOWER ELEVATOR / Tower system ?

     Like this:

pastedImage_4.png

pastedImage_5.png

Can it convert the PCIe interface to the General Purpose Input/Output(GPIO)?

Looking for your further reply. Have a good day.

 

qzy

0 Kudos
Reply
1 Solution
1,469 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,

Yes, you are correct the Tower elevator can convert  the PCIe interface to GPIOs. Also, another purpose of the Tower elevator is to interconnect boards with each other. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

View solution in original post

0 Kudos
Reply
2 Replies
1,470 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello,

Yes, you are correct the Tower elevator can convert  the PCIe interface to GPIOs. Also, another purpose of the Tower elevator is to interconnect boards with each other. 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply
1,469 Views
qzy_perfect
Contributor III

Hello Victor,

Thanks for your reply.

Have a good day.

qzy

0 Kudos
Reply