Hello,
I use SDK_2.0_MK64FN1M0xxx12 the I2C routines for communication, but when I put the hosts set I2C1, the slave is set to I2C0, the two can not communicate properly, why? (SPI also have the same situation)
P.S:The code is downloaded from the NXP,and nothing modification.Accessory is the code for I2C and SPI
Look forward to answer.
各位好:
我使用SDK_2.0_MK64FN1M0xxx12中的I2C例程进行通信,但是当我把主机设为I2C1,从机设置为I2C0时,这两个没法正常通信,请问这是为什么?(SPI也有同样的情况)
附件是我从NXP下载下来的例程代码
期待各位的回复。
Original Attachment has been moved to: dspi_interrupt.zip
Original Attachment has been moved to: I2C_interrupt.zip