What is the behavior of the IO when the device is unpowered?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the behavior of the IO when the device is unpowered?

ソリューションへジャンプ
1,430件の閲覧回数
leehonaker
Contributor I

I have a board with an MK60FX512VLQ15 on it with IO connected as control inputs to an LTM4609 DC/DC Regulator. When the uC is not powered, the IO appear to be logic '0' to the regulator. Unfortunately this regulator supplies power to the uC and the active low state is preventing it from turning on.

Does anyone know if the IO of an unpowered device are supposed to behave this way?

Thanks,

Lee

ラベル(1)
0 件の賞賛
返信
1 解決策
1,377件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Lee Honaker:

Not sure I understand your setup.

- Does the MK60 control de regulator to turn off its own power but then you want the regulator to enable on its own?

- Can you share a schematic of your connections so we understand better?

When the MCU is not powered it does not drive the pins in either high or low level, so the behavior is unpredictable, you cannot rely on the pin to use it as a control signal. Maybe what you need is some kind of gate or a double pole switch to turn on the board and once the MCU started you can control the regulator with a pin.

Regards!

Jorge Gonzalez

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,378件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Lee Honaker:

Not sure I understand your setup.

- Does the MK60 control de regulator to turn off its own power but then you want the regulator to enable on its own?

- Can you share a schematic of your connections so we understand better?

When the MCU is not powered it does not drive the pins in either high or low level, so the behavior is unpredictable, you cannot rely on the pin to use it as a control signal. Maybe what you need is some kind of gate or a double pole switch to turn on the board and once the MCU started you can control the regulator with a pin.

Regards!

Jorge Gonzalez

0 件の賞賛
返信
1,377件の閲覧回数
leehonaker
Contributor I

Thanks Jorge. I agree, you can't predict the behavior of the IO when the MCU is unpowered. I recommended placing a pulldown on the control signal which would enable the regulator (active low enable) until the MCU was powered and configured. Sorry I didn't get back to you sooner, but I took an extended Christmas break!

God Bless,

Lee

0 件の賞賛
返信