Hi Eunseok,
I think no matter using the polling mode or interrupt mode is Ok for MCU to receive the data from the PC correctly.
The key of the communication is guaranteeing the process follow the corresponding protocol.
I'd like to suggest that you can refer to AN2295 note and its code for details which share an example of serial bootloader.
Please learn more details about them through the link as below.
http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf
cache.freescale.com/files/microcontrollers/doc/app_note/AN2295SW.zip
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------