What is BSP and PSP ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is BSP and PSP ?

8,243件の閲覧回数
Glogov_Kolac
Contributor II

Can someone explain me the meaning of theese terms. I am new in CORTEX M4 ?

4 返答(返信)

4,675件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

See http://www.freescale.com/files/32bit/doc/app_note/AN4287.pdf for BSP (Board Support Packages)

 

PSP is not defined there but I am guessing that it may mean Project Support Package(?)

 

Regards

 

Mark

 

0 件の賞賛
返信

4,675件の閲覧回数
Nouchi
Senior Contributor II

Hi,

 

IMHO, PSP means Processor Support Package ?

 

Regards,

 

Emmanuel

4,675件の閲覧回数
Glogov_Kolac
Contributor II

It isunbelievable that there is no official explanation by Freescale of theese 2 terms !

0 件の賞賛
返信

4,675件の閲覧回数
Dekiru
Contributor IV

Hi Kolac,

 

Freescale mentions that in Glossary section of MQX User Guide (MQXOG.pdf)

 

BSP

Board support package. A group of files that are specific to a particular type of processor on a particular type of board. It includes drivers.

 

PSP

Processor Support Package. A group of file that are specific to a CPU type.

Regards