Hi Brent,
Do you want to have the connector or socket which can put the K22F chip to your board? And you don't want to solid the K22F chip directly to the board?
If yes, you should check your K22F part number, then refer to the package to find the according chip socket.
If not, please tell me the detail function of your connector, then I can help you to answer it.
About the programmer, you can use P&E CycloneMAX:
P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...
Wish it helps you!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------