What connector do we need to use with the K22F series chip-set when laying out a board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What connector do we need to use with the K22F series chip-set when laying out a board?

跳至解决方案
1,544 次查看
brentgreenwald
Contributor III

If we lay out our own circuit board with a  on it, what connector do we need to put on the circuit board and what programmer do we need to buy?

0 项奖励
回复
1 解答
1,306 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Brent,

    Do you want to have the connector or socket which can put the K22F chip to your board? And you don't want to solid the K22F chip directly to the board?

    If yes, you should check your K22F part number, then refer to the package to find the according chip socket.

    If not, please tell me the detail function of your connector, then I can help you to answer it.

  About the programmer, you can use P&E CycloneMAX:

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Wish it helps you!


Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,307 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Brent,

    Do you want to have the connector or socket which can put the K22F chip to your board? And you don't want to solid the K22F chip directly to the board?

    If yes, you should check your K22F part number, then refer to the package to find the according chip socket.

    If not, please tell me the detail function of your connector, then I can help you to answer it.

  About the programmer, you can use P&E CycloneMAX:

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Wish it helps you!


Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,306 次查看
brentgreenwald
Contributor III

Is their any cheaper programmers for the K22F chip set? I'm on a budget for my research and I am trying to find something around $120 at most.

0 项奖励
回复
1,306 次查看
mjbcswitzerland
Specialist V

Brent

If you have a tight budget you can use  FRDM-K22F board to program production boards with - either using the SWE interface of ist OpenSDA debgger or else using it as EzPort programmer.

See the following (and video there) showing how EzPort production programming is possible even without a connector: EzPort Cloning

Regards

Mark