What are the routines to identify neutral disturbances in MKM34Z series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the routines to identify neutral disturbances in MKM34Z series

1,027件の閲覧回数
panneerrajangun
Contributor I

Hi,

How to read and identify the Neutral disturbance tamper in firmware (MKM34Z/33Z series) for Single phase energy meter application. Please suggest.

Thanks & Regards,

Rajan

0 件の賞賛
返信
1 返信

887件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear panneerrajangunasekaran,

I apologize for the delay, regarding to your question:

For neutral tampering, you need to measure not only current in phase but also neutral current.

 

Then meter can detect external connecting load to ground or reverse load wire connection.

 

If neutral is disconnected completely so the meter loses supply voltage then power meter electronics must use an internal battery and wakeup from time to time to check whether some current consumption is detected even under no presence of supply voltage on phase shunt resistor.

 

Please check  the following application note: http://www.nxp.com/assets/documents/data/en/application-notes/AN4993.pdf

BR

Jonathan

0 件の賞賛
返信