What are the jumper settings for CAN on the K65?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What are the jumper settings for CAN on the K65?

464 次查看
josephjean-jacq
Contributor III

Hello everyone,

I was looking through the quick start guide and the datasheet for the K65 to find the jumper settings for CAN. I was able to find it for UART, I2C, etc, but not for CAN.

I was wondering do I need to purchase the K65 tower module with a separate extension card that comes with the two CAN communication interface buses that K65 supports?

Would the setup be similar to the following video - FlexCAN demonstration on K60 Tower Kit

Any help is greatly appreciated!!

0 项奖励
回复
1 回复

363 次查看
miduo
NXP Employee
NXP Employee

Hello,

From the user manual of TWR-K65F108M, it mentioned:

pastedImage_1.png

pastedImage_2.png

So the pins for FLEXCAN are within the elevator connectors.

0 项奖励
回复