Hello guys,
 I wonder how to use an RTOS in FRDM-KE06Z in KDS go on a baremetal project.
 Is that possible?
 It seems that the MQX does not support this hardware.
 Thanks,
已解决! 转到解答。
Hi Jeferson,
I'm using FreeRTOS with that board. Attached is a project which is available as well on SourceForge (mcuoneclipse/Examples/KDS/FRDM-KE06Z/FRDM-KE06Z at master · ErichStyger/mcuoneclipse · GitHub ).
This project is using Processor Expert (without Kinetis SDK). The project uses McuOnEclipse components available from SourceForge (see McuOnEclipse Releases on SourceForge | MCU on Eclipse ). You can use that FreeRTOS port without Processor Expert too (bare).
I hope this helps,
Erich
MQX-Lite is supported on the KE06, though you use it through Processor Expert. I haven't had experience with the other ones mentioned, but I have been using MQX-Lite on the KE06 for over a year now.
Hi
For a solution that will allow a project to run on most processors from KE02 up to K80 see
http://www.utasker.com/kinetis/FRDM-KE06Z.html
Regards
Mark
Thank you,
I am using the IDE KDS and must rtos who is supported in project of type baremetal, without using KSDK.
I tried portable BRTOS system, but without success.
I did not understand how portable FreeRTOS for this IDE.
If you have any idea, I would be very grateful.
Hi Jeferson,
I'm using FreeRTOS with that board. Attached is a project which is available as well on SourceForge (mcuoneclipse/Examples/KDS/FRDM-KE06Z/FRDM-KE06Z at master · ErichStyger/mcuoneclipse · GitHub ).
This project is using Processor Expert (without Kinetis SDK). The project uses McuOnEclipse components available from SourceForge (see McuOnEclipse Releases on SourceForge | MCU on Eclipse ). You can use that FreeRTOS port without Processor Expert too (bare).
I hope this helps,
Erich