I do not know to connect the DC voltage supply. The board has two green and two red ports, and another two black(ground?) ports. None of the ports are labeled and I could not find a document that explains the connections. Thanks.
Typical color codding is as follow:
Green ports are Vgs bias.
Red ports are Vds power.
Black ports are GND.
Power-Up Sequence
1. Terminate the RF input and output with 50 Ohm impedances: no RF signal applied.
2. Dial all Vgs for minimum voltage.
3. Set-up Vds over-current protection at the max expected level (~40A). Apply 50V Vds supply across the VDD and GND terminals.
4. Slowly dial-up Vgs until the expected portion of IDQ is seen flowing from Vds. The order of adjustment is not important.
6. Apply RF signal and load.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------