Way to "attach" a project to a specific FRDM-KL27Z board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Way to "attach" a project to a specific FRDM-KL27Z board?

639 Views
rickstuart
Contributor V

Hi...

I'm developing on 2 FRDM-KL27Z boards at the same time.  It's simple enough to have 2 workbench sessions running at the same time.  Just have to unplug everything (USB) then load & plug in each matching project & board.  One pair at a time.  But it would be nice to load a project and have it "know" which board to "attach" to.  There a way to do that?

-thanks

0 Kudos
3 Replies

521 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Rick Stuart:

For this kind of question it is important that you mention the IDE (KDS, IAR, Keil).

As mentioned by Erich, the behavior will depend on the interface connection (Segger, P&E, CMSIS-DAP) and also in the IDE debugger features/configurations for that particular connection.

Regards!

Jorge Gonzalez

0 Kudos

521 Views
rickstuart
Contributor V

Sorry, I am using the IAR Embedded Workbench for ARM version 7.40.1.8472.  The USB interface(s) are the ones offered up by the 2nd communication processor on the FRDM-KL27Z board.

-thanks

0 Kudos

521 Views
BlackNight
NXP Employee
NXP Employee

Hi Rick,

Do you mean 'attach to a running target'? If so, then this might be helpful: Attaching to a Running Target with Segger J-Link, GDB and Eclipse | MCU on Eclipse

If you want to 'fix' the USB port to the run control device: that will depend on the run control (like P&E).

As for P&E and Segger, you can select the USB ID of the device in the launch configuration.

Erich

0 Kudos