Watchdog of KEA-128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog of KEA-128

539 Views
vigneshbalaji
Senior Contributor I

Hi,

    I want to know Which is the best Clock Source for Watchdog of KEA-128? Is it Bus clock or Internal 32 khz crystal or Internal LPO 1 Khz or External Clock?

0 Kudos
1 Reply

325 Views
isaacavila
NXP Employee
NXP Employee

Hello Vignesh,

It depends on your safety requirments (if you want to use internal reference or external, timeout value, etc.), but basically using a clock source other than the bus clock ensures that the watchdog counter continues to run if the bus clock is somehow halted (you can check Backup reset feature on page 220 from Reference manual for more details).

Next table also sumarizes different time-out values according the selected reference clock (both enabling or disabling prescaler) so it could help you to meet your requirements:

Watchdog timeout availability.jpg

I hope this can help you!

Regards,

Isaac

0 Kudos