Hello,
I am using ksdk 1.3 with processor expert.
I can't reach a breakpoint on the Watchdog ISR.
As far as I can tell, the LPO clock is set to 1kHz as described in the reference manual.
const wdog_config_t watchdog1_InitConfig0 = {
.wdogEnable = true,
.clkSrc = kWdogLpoClkSrc,
.prescaler = kWdogClkPrescalerDivide1,
.workMode.kWdogEnableInWaitMode = true,
.workMode.kWdogEnableInStopMode = true,
.workMode.kWdogEnableInDebugMode = false,
.updateEnable = true,
.intEnable = true,
.winEnable = false,
.windowValue = 0U,
.timeoutValue = 10000U,
};
I have tried configuring the interrupt at compile and at runtime, I can't seem to reach it.
I looked at WDOG_STCTRLL and I never saw bit 15 (INTFLG) rise. I put a breakpoint on the reset handler to see if the watchdog interrupt was ever raised.
What am I missing here?
Regards,
Jason
Ivan,
That did not make a difference. I will keep it enabled though.
I feel like my watch dog is hitting that second reset quicker than I can get to the interrupt.
Even setting the priority of the interrupt to 0 (Maximal Cortex-M4) I don't seem to hit it.
LPO Clock 1kHz
Prescaler 1
Bus Clock 20.97 MHz
Should I try to slow down the LPO clock so I don't hit the second reset so quickly?
Best Regards,
Jason