Wake up on GPIO on k21F(MK21FX512VMC12)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wake up on GPIO on k21F(MK21FX512VMC12)

1,036件の閲覧回数
savinaydharmapp
Contributor I

Hi All,

My application is configured to wake up on external event on GPO(i.e PTC11).  Proccessor is not waking up when i enter sleep

_lpm_set_operation_mode (LPM_OPERATION_MODE_SLEEP);. where as i am able to wakeup when enter LPM(low power mode) using 

_lpm_set_operation_mode (LPM_OPERATION_MODE_WAIT);. Could anyone guide to reslove the issue.

Regards

savinay

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

959件の閲覧回数
cutworth
NXP Employee
NXP Employee

Hi Savinay,

Are you trying to run the code with "lowpower" demo under MQX folder? Which MQX version you use? Are you running this with Freescale tower board or with your own board? If you are running with your own board, did you port the BSP?

If you have written your own low power entry code, then please share your code.

Hao

0 件の賞賛
返信

959件の閲覧回数
savinaydharmapp
Contributor I

Hi Hao,

We are using our own board. BSP is ported to this board. We are using lpm api provided by BSP to enter low power mode.

Regards

savinay

0 件の賞賛
返信