Using of Flexbus CS1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using of Flexbus CS1

1,182 Views
durgasivakrishn
Contributor III

Hi,

    I am using MK66FN2M0VLQ18 microcontroller. By this controller, I am interfacing external memory(MIL-STD1553) using flexbus module. if I use CS0(pin No 128) it is working fine but I want to use CS1(pin No 127) with this configuration it is not working. Can you explain  how to use CS1 for accessing external memory module by flexbus

                        waiting for your suggestions.

With Regards,

Sivakrishna

Tags (3)
0 Kudos
Reply
2 Replies

1,111 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sivakrishna,

I have checked the pin assignment of MK66FN2M0VLQ18, the FB_CS1 is multiplexed with PTD0 pin, this is the process to configure the pin as FB_CS1.

1)enable PORTD clock by SIM_SCGC5|=0x01<<12;

2)configure MUX to configure the pin as FlexBUS

PORTD_PCR0&=~(0x07<<8);

PORTD_PCR0|=0x05<<8;

3)configure the FB_CS1 as FB_CS1 with the code

FB_CSPMCR|=0x01<<28; //set Group1 as 01;

4)set the FB_CSAR1 address as 0x6000 0000;

5)set the FB_CSMR1=0x01; //which is based on the size of external memory size for BAM bits, //set the bit0  as 1

6)set the other FB registers

Pls have a try.

Hope it can help you

BR

Xiangjun rong

0 Kudos
Reply

1,111 Views
durgasivakrishn
Contributor III

Hi,Xiangjun rong

            Thanks for your support and response I will check and let to know

With Regards,

Sivakrishna

0 Kudos
Reply