Hello every one. I am trying to use the DMA to store the ADC results into a buffer and then to a file. I found AN4590 application note useful but its in IAR IDE. How ever I am working on Coderwarrior 10.5. Does any one know how to migrate from it? or suggest any likely example which could illustrate the configuration and use of DMA.
Regards
Abdullah
已解决! 转到解答。
Abdullah
Binary (or SREC) files can be loaded using the Flash utility in CodeWarrior 10.x (look for the symbol with the flash of lightning in the menu bar). It is not necessary to import such files to the project.
Regards
Mark
Hi Ping,
As soon as i am running the code on my CW 10.5, the compiler is giving me cpu interrupt. However if i create the project once again with Process Expert in CW.10.5, its working but DMA isnot being enable that is DMA_flag is always zero.
I am just creating a new project in PE, and then copy your components to my one and Generating the code.
Any remedy?
Regards
Abdullah
Hi Abdullah,
In your email you mentioned that the DMA_flag is always keep zero. I'd like to confirm that whether you had connected the TTA8 with PTC1 or PTC2 when you tested the democ code.
I'd like to suggest that you use the export and inport feature of PE which could make you create a new project easily and quickly and I''ve included the proceesor expert usr guide in the reply, so please refer to it.
That's all and I'm looking forward to your reply.
Have a nice day!
Best regards,
Ping
Hi
See Application note on DMA driven ADC and DAC, using PDB as timebase
This implementation is compatible/works with IAR, Keil, GCC, Rowley Crossworks and CW10.x.
Regards
Mark
Hi Mark!
Thanks for the info.
The software link you have given contains a .bin file. When importing it to codewarrior it expects .elf format or so. or if you can let me know the procedure for importing if i am wrong.
Waiting for your reply
Abdullah
Binary (or SREC) files can be loaded using the Flash utility in CodeWarrior 10.x (look for the symbol with the flash of lightning in the menu bar). It is not necessary to import such files to the project.
Regards
Mark