Unreliable J-link flashing to KL16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unreliable J-link flashing to KL16

跳至解决方案
3,078 次查看
jacobjennings
Contributor III

In a previously working configuration, I can't seem to successfully flash. I see "block verification error" and "Can not read register 0 (R0) while CPU is running". Any thoughts?

SEGGER J-Link GDB Server V4.98b Command Line Version

JLinkARM.dll V4.98b (DLL compiled Apr 10 2015 20:35:16)

-----GDB Server start settings-----

GDBInit file:                  none

GDB Server Listening port:     2331

SWO raw output listening port: 2332

Terminal I/O port:             2333

Accept remote connection:      localhost only

Generate logfile:              off

Verify download:               on

Init regs on start:            on

Silent mode:                   off

Single run mode:               on

Target connection timeout:     0 ms

------J-Link related settings------

J-Link Host interface:         USB

J-Link script:                 none

J-Link settings file:          none

------Target related settings------

Target device:                 MKL16Z128xxx4

Target interface:              SWD

Target interface speed:        1000kHz

Target endian:                 little

Connecting to J-Link...

J-Link is connected.

Firmware: J-Link V9 compiled Mar  2 2016 14:43:29

Hardware: V9.30

S/N: 59306698

Feature(s): GDB

Checking target voltage...

Target voltage: 1.83 V

Listening on TCP/IP port 2331

Connecting to target...Connected to target

Waiting for GDB connection...Connected to 127.0.0.1

Reading all registers

Read 4 bytes @ address 0x00000000 (Data = 0x20003000)

Target interface speed set to 1000 kHz

Resetting target

Halting target CPU...

...Target halted (PC = 0x0000A934)

R0 = FFFFFFFF, R1 = F000300C, R2 = 00000400, R3 = 20003000

R4 = FFFFFFFF, R5 = 00000000, R6 = 000000FF, R7 = 1FFFF161

R8 = FBFFF2FF, R9 = FF6FFFE7, R10= FFFF6EFF, R11= BFFFFFFD

R12= BDEFBFFC, R13= 20003000, MSP= 20003000, PSP= FFDFF77C

R14(LR) = FFFFFFF9, R15(PC) = 0000A934

XPSR A1000000, APSR A0000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Target interface speed set to 1000 kHz

Flash breakpoints enabled

Semi-hosting enabled (VectorAddr = 0x08)

Semihosting I/O set to TELNET Client

SWO disabled succesfully.

SWO enabled succesfully.

Downloading 192 bytes @ address 0x00000000 - Verified OK

Downloading 16000 bytes @ address 0x00000410 - Verified OK

Downloading 15856 bytes @ address 0x00004290 - Verified OK

Downloading 16048 bytes @ address 0x00008080 - Verified OK

Downloading 16240 bytes @ address 0x0000BF30 - Verified OK

Downloading 16240 bytes @ address 0x0000FEA0 - Verified OK

Downloading 900 bytes @ address 0x00013E10 - Verified OK

Downloading 8 bytes @ address 0x00014194 - Verified OK

Downloading 8 bytes @ address 0x0001419C - Verified OK

Downloading 4 bytes @ address 0x000141A4 - Verified OK

Downloading 112 bytes @ address 0x000141A8 - Verified OK

Downloading 24 bytes @ address 0x00014218 - Verified OK

Read 4 bytes @ address 0x0000A934 (Data = 0x1C184B09)

Read 2 bytes @ address 0x0000A41A (Data = 0xF7FF)

Read 2 bytes @ address 0x0000A41A (Data = 0xF7FF)

Comparing flash   [....................] Done.

Erasing flash     [....................] Done.

Programming flash [....................] Done.

ERROR: Programming failed @ address 0x0000A400 (block verification error)

Verifying flash   [....................] Done.

Resetting target

Halting target CPU...

...Target halted (PC = 0x0000A934)

Read 2 bytes @ address 0x0000A41A (Data = 0xF7FF)

Read 2 bytes @ address 0x0000A41A (Data = 0xF7FF)

Read 2 bytes @ address 0x0000A41A (Data = 0xF7FF)

R0 = 00000050, R1 = F000300C, R2 = 0000A400, R3 = 00000200

R4 = BD38601A, R5 = 00000000, R6 = 000000FF, R7 = 1FFFF161

R8 = FBFFF2FF, R9 = FF6FFFE7, R10= FFFF6EFF, R11= BFFFFFFD

R12= BDEFBFFC, R13= 20003000, MSP= 20003000, PSP= FFDFF77C

R14(LR) = 1FFFF159, R15(PC) = 0000A934

XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Read 4 bytes @ address 0x0000A934 (Data = 0x1C184B09)

Setting breakpoint @ address 0x0000A41A, Size = 2, BPHandle = 0x0002

Starting target CPU...

ERROR: Can not read register 15 (R15) while CPU is running

...Target halted (PC = 0x00000000)

Reading all registers

ERROR: Can not read register 0 (R0) while CPU is running

ERROR: Can not read register 1 (R1) while CPU is running

ERROR: Can not read register 2 (R2) while CPU is running

ERROR: Can not read register 3 (R3) while CPU is running

ERROR: Can not read register 4 (R4) while CPU is running

ERROR: Can not read register 5 (R5) while CPU is running

ERROR: Can not read register 6 (R6) while CPU is running

ERROR: Can not read register 7 (R7) while CPU is running

ERROR: Can not read register 8 (R8) while CPU is running

ERROR: Can not read register 9 (R9) while CPU is running

ERROR: Can not read register 10 (R10) while CPU is running

ERROR: Can not read register 11 (R11) while CPU is running

ERROR: Can not read register 12 (R12) while CPU is running

ERROR: Can not read register 13 (R13) while CPU is running

ERROR: Can not read register 14 (R14) while CPU is running

ERROR: Can not read register 15 (R15) while CPU is running

ERROR: Can not read register 16 (XPSR) while CPU is running

ERROR: Can not read register 17 (MSP) while CPU is running

ERROR: Can not read register 18 (PSP) while CPU is running

ERROR: Can not read register 24 (PRIMASK) while CPU is running

ERROR: Can not read register 25 (BASEPRI) while CPU is running

ERROR: Can not read register 26 (FAULTMASK) while CPU is running

ERROR: Can not read register 27 (CONTROL) while CPU is running

Removing breakpoint @ address 0x0000A41A, Size = 2

WARNING: Failed to read memory @ address 0x00000000

Read 4 bytes @ address 0x00000000 (Data = 0x20003000)

标签 (1)
0 项奖励
回复
1 解答
2,536 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jacob,

The SWD_CLK pin has an internal pull down and SWD_DIO has an internal pull up. But an external 4.7 kΩ to 10 kΩ pullup is recommended on SWD_DIO. You can refer the 10-pin debug interface below.

10-pin debug interface.jpg

And the RESET_b and NMI_b should be care.

RESET_b and NMI_b.jpg

Best Regards,

Robin

在原帖中查看解决方案

2 回复数
2,537 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jacob,

The SWD_CLK pin has an internal pull down and SWD_DIO has an internal pull up. But an external 4.7 kΩ to 10 kΩ pullup is recommended on SWD_DIO. You can refer the 10-pin debug interface below.

10-pin debug interface.jpg

And the RESET_b and NMI_b should be care.

RESET_b and NMI_b.jpg

Best Regards,

Robin

2,536 次查看
jacobjennings
Contributor III

Resolved: Needed 10k pullup on SWD clk and SWD reset, pulldown on clock

0 项奖励
回复