Understanding the Kinetis HEX file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Understanding the Kinetis HEX file

跳至解决方案
1,432 次查看
sfarzan
Contributor I

Hi everybody,

I'm trying to understand the hex file created by CodeWarrior for KL16. The hex file has the following structure:

:10000000000C00206D31000025310000253100007A

:1000100000000000000000000000000000000000E0

:10002000000000000000000000000000253100007A

:100030000000000000000000253100002531000014

:100040002531000025310000253100002531000058

:10005000000000002531000025310000253100009E

:100060002531000025310000253100002531000038

...

:106C3000306C000000FCFF1F00000000000000009E

:086C400000000000000000004C

:040000030000316D5B

:00000001FF

I know that second and third bytes show the address following by 1 byte (?) and then 16 bytes of code and finally another extra byte (?).

It seems the last three lines don't have this structure. Could you please tell me what these three lines refer to?

Thanks in advance.


标签 (1)
0 项奖励
回复
1 解答
1,206 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复
1 回复
1,207 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复