USB0_DP and USB0_DM when USB not used - K60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB0_DP and USB0_DM when USB not used - K60

跳至解决方案
2,143 次查看
igw
Contributor II

On a K60F what should we do with the USB0_DP and USB0_DM pins when we aren't using the USB peripheral?

There doesn't seem to be any guidance in the datasheet or user manual.

I was thinking that we would pull them down to GND lightly.  Or should we pull them up lightly?

Thanks,

Ian

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,806 次查看
wenlongzhang
Contributor II

just put both of them to GND is OK.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,807 次查看
wenlongzhang
Contributor II

just put both of them to GND is OK.

0 项奖励
回复
1,806 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Ian,

Thank you very much for your focus on Freescale Kinetis product. I'm glad to provide service for you.

It's ok to pull the USB0_DP and USB0_DM pins down to GND.


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------