USB OTG connection diagram

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB OTG connection diagram

跳至解决方案
1,627 次查看
javierhernande1
Contributor IV

Hello,

Is there an example of how to connect K2x MCU family to USB Type-C connector with OTG support? I have not found anything.

Best regards

usb.png

标签 (2)
1 解答
1,366 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Javier,

If you need full USB type C function support, you have use some chip like CC logic for USB Type-C applications|NXP besides Kinetis K2x, but if you just need a USB type C connection, you may connect the signals that K2x USB FS OTG has and leave other unused signals unconnected.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,367 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Javier,

If you need full USB type C function support, you have use some chip like CC logic for USB Type-C applications|NXP besides Kinetis K2x, but if you just need a USB type C connection, you may connect the signals that K2x USB FS OTG has and leave other unused signals unconnected.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,366 次查看
javierhernande1
Contributor IV

just at a USB type C connection.

Thanks very much.

0 项奖励
回复