I am using USB v3.2.0 stack.
Steps I followed
1. Navigate to the project folder (s08usbjm60) and locate the CodeWwarrior10 project file (.project).
2. Open the project by dragging the .project file and dropping it into the CodeWarrior 10 project
space.
3. After you have opened the project, the following window appears. To build the project choose
"Build Project" from the Project menu.
And here I am getting following error.
| Description | Resource | Path | Location | Type |
| make: *** [Source/driver/usb_dci_c.obj] Error 1 | s08usbjm60 | line 0 | C/C++ Problem |
Hi Karthik,
I'd like to suggest that you should check whether the CW10.1 had already installed the package that be applicable to S08 or not.
Hope it helps.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------