USB 4.1.1 USBERR_DEVICE_BUSY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB 4.1.1 USBERR_DEVICE_BUSY

497件の閲覧回数
Mike_d
Contributor IV

Hi,

I often end up with a USBERR_DEVICE_BUSY error from using the USB_Class_CDC_Interface_DIC_Send_Data() function.

How do I recover my interface at this point?

Thanks,

-Mike

0 件の賞賛
返信
1 返信

379件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mike,

Thanks for your interest in NXP Semiconductor products and the opportunity to serve you.

I was wondering if you can illustrate the detail procedure to replicate the issue, then it will help me to investigate the issue.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信