Ok, Mark. Thank you.
Unfortunately, your bin does not work wither, which lead me to believe that something with my setup is wrong.
I've connected the FRDM as follows:
The small board below is an RS485 to UART. The UART RX is connected to J2/4 (TX), the UART TX is connected to J1/16 (RX).
GND & Vcc is connected to J199 GND & Vcc (I've left it there because I've used to work through UART4 - works great with that setup, now I want to move to UART1).
Any idea you can think off?
What you referred to 'respond to input with a command line menu)' will also be seen in the Real term, when clicking something or only with your GUI? How do I download your GUI?
Thanks,
Roy

Ok,here's an update:
Using your bin, when I reset the board, I get on my Real term:
'rs 485 example'
But they are shown when I'm connected to the UART of the OpenSDA (UART0). I've double checked it. In UART1 (where my RS485 to UART is connected) I don't get anything.
I even disconnected my USB dongle (which converts USB to RS485, and then it goes to the small board) and still, when reset is clicked I get this string in Real term.
Thanks anyway for your help.
Roy