UART on kl25z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART on kl25z

跳至解决方案
3,169 次查看
aayushm
Contributor I

What is the differnce  between UART0, UART1, UART2 on kl25z ?

What is the operating voltage of RX/TX pin of kl25z ?

0 项奖励
回复
1 解答
1,654 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Aayush

UART0 is a special UART module. It can support basic UART with DMA interface function, x4 to x32 oversampling of baud-rate.This module supports LIN slave operation.

The module can remain functional in VLPS mode provided the clock it is using remains enabled. It can support ISO7816.

UART1 and UART2 are basic universal asynchronous receiver/transmitter (UART) modules with DMA function support. Generally, these modules are used in RS-232, RS-485, and other communications. This module supports LIN Slave operation.

UART pins are digital. So the operation voltage depends on VDD voltage value.

Hope my reply can help you.

Best Regards

Paul

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,655 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Aayush

UART0 is a special UART module. It can support basic UART with DMA interface function, x4 to x32 oversampling of baud-rate.This module supports LIN slave operation.

The module can remain functional in VLPS mode provided the clock it is using remains enabled. It can support ISO7816.

UART1 and UART2 are basic universal asynchronous receiver/transmitter (UART) modules with DMA function support. Generally, these modules are used in RS-232, RS-485, and other communications. This module supports LIN Slave operation.

UART pins are digital. So the operation voltage depends on VDD voltage value.

Hope my reply can help you.

Best Regards

Paul

0 项奖励
回复