Hi
I am using K21 controller(Baremetal). When I try to write some bytes to UART0, it is writing junk bytes. I tapped the data and checked. But for the second time it is writing complete data correctly.
Can anyone please help me
 
					
				
		
I apologize for reviving this old thread. However, i'm in the same boat. Below is the link to the question i had
Kinetis K64 UART0 Baud Issue ?
Thanks
Vu
Any solution you got chandra?
Team Freescale is there is any problem in driver. I am running with same problem.
Using MQX4.2 Codewarrior 10.6.
Hi,
It worked with the UART4 without any glitch. But with UART0 it doesnt work as expected. I think it has some baud issues.
Thanks ,
Chandra
Hi Zhe TIan,
Yes I have checked the clock settings and I am giving it right. UART0 is giving problem for the first time only. I have already attached the code.
It is behaving the same way in MQX also.
Regards,
Chandrasekhar
I know that this is an older post but I ran into a similar issue with UART5 on a k64 TWR board recently. I started out testing at 2400 baud and periodically received junk characters. I cycled power to the board and it sometimes worked correctly and other times not. I was sending 'A' through 'G' characters (0x41 through 0x47). The junk characters received were the actual characters, but not shifted correctly. For example:
'A' = 01000001 came across as 00001011,
'B' = 01000010 came across as 00010011,
'C' = 01000011 came across as 00011011, etc.
When I changed the baud rate up to 9600 or higher (I went all the way up to 600,000 baud) it worked perfectly. I suspect that it was just a timing issue in the way I set up the baud rate. If I had used Processor Expert I could have fine tuned the Baud Rate and it would have worked better at 2400 baud.
I was using some example code that I found on a forum somewhere else. (pasted below) I modified it to use the UART5_RX_TX_IRQn interrupt.
John Baker
--------------------------------------------------------------------------------------------------------------------------------------------------
void UART_Init ( UART_Type *pUART ){
uint16_t u16Sbr, u16Brfa;
uint8_t u8Temp;
uint32_t u32SysClk = 120000;
uint32_t u32Baud = UART_BAUDRATE;
/* Enable the clock to the selected PORT */
SIM->SCGC5 |= SIM_SCGC5_PORTE_MASK;
/* Set the pins multiplexer to UART RX/TX mode */
PORTE->PCR[8] = PORT_PCR_MUX( 3 );
PORTE->PCR[9] = PORT_PCR_MUX( 3 );
/* Enable the clock to the selected UART */
SIM->SCGC1 |= SIM_SCGC1_UART5_MASK;
/* Make sure that the transmitter and receiver are disabled while we
* change settings.
*/
pUART->C2 &= ~(UART_C2_TE_MASK | UART_C2_RE_MASK );
/* Configure the UART for 8-bit mode, no parity */
pUART->C1 = 0;
/* Calculate baud settings */
//u16Sbr = (((u32SysClk)>>4) + (u32Baud>>1))/u32Baud;
u16Sbr = (uint16_t)((((u32SysClk*1000)>>5))/u32Baud);
/* Save off the current value of the UARTx_BDH except for the SBR field */
u8Temp = pUART->BDH & ~(UART_BDH_SBR_MASK);
pUART->BDH = u8Temp | UART_BDH_SBR(((u16Sbr & 0x1F00) >> 8));
pUART->BDL = (uint8_t)(u16Sbr & UART_BDL_SBR_MASK);
/* Determine if a fractional divider is needed to get closer to the baud rate */
u16Brfa = (((u32SysClk*32000)/(u32Baud * 16)) - (u16Sbr * 32));
/* Save off the current value of the UARTx_C4 register except for the BRFA field */
u8Temp = pUART->C4 & ~(UART_C4_BRFA(0x1F));
pUART->C4 = u8Temp | UART_C4_BRFA(u16Brfa);
/* Enable interrupt */
NVIC_SetPriority(UART5_RX_TX_IRQn,64);
NVIC_ClearPendingIRQ(UART5_RX_TX_IRQn);
NVIC_EnableIRQ(UART5_RX_TX_IRQn);
pUART->C2 |= UART_C2_RIE_MASK;
/* Enable receiver and transmitter */
pUART->C2 |= ( UART_C2_TE_MASK | UART_C2_RE_MASK );
}