UART DMA and CTS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART DMA and CTS

跳至解决方案
1,531 次查看
lsrbigfoot
Contributor IV

Does the UART-CTS input signal (when activated) have the ability to block/unblock UART-Tx DMA traffic automatically (without processor intervention)?

If not, then what extra controls are required to make this happen?

标签 (1)
0 项奖励
回复
1 解答
1,357 次查看
mjbcswitzerland
Specialist V

Hi

Check the UART MODEM register for the part type that you are using.

The control bit TXCTSE enables CTS control of the transmitter, which also pauses DMA transmission.

Regards

Mark

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,358 次查看
mjbcswitzerland
Specialist V

Hi

Check the UART MODEM register for the part type that you are using.

The control bit TXCTSE enables CTS control of the transmitter, which also pauses DMA transmission.

Regards

Mark

0 项奖励
回复