Two I2C interfaces AND MDIO / MDC possible?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Two I2C interfaces AND MDIO / MDC possible?

2,636 次查看
pk2
Contributor III

I am working on a design that requires an RMII Ethernet interface and two I2C interfaces (one master and 1 slave).  Will the MK60FN1M0VLQ12 support this?  WIll the MDIO / MDC interface (pins 81 and 82 for this device) and both I2C0 and I2C1 work at the same time (i.e. simultaneously)?

标签 (1)
0 项奖励
回复
3 回复数

1,678 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, PK2

No, you can use I2C and RMII at the same time. I suggest you use Pin 137,138 for I2C0.

Hope my reply can help you.

Best Regards

Paul

1,678 次查看
pk2
Contributor III

Is there a reason I can not use pins 83 and 84?

0 项奖励
回复

1,678 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, PK2

Yes, you can use pin 83 and 84.