Trouble with K10 programming with JTAG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Trouble with K10 programming with JTAG

跳至解决方案
1,725 次查看
gfritz
Contributor II

Hi everyone,

I have problems to establish communication between K10 and jtag probe. I use 2 differents probe : an Olimex ARM-USB-OCD-H and a Segger JLink. Both are used with OpenOCD on Linux and windows. And with both, I obtain that same error message :

Error: JTAG scan chain interrogation failed: all zeroes

Error: Check JTAG interface, timings, target power, etc.

Error: Trying to use configured scan chain anyway...

Error: k10.cpu: IR capture error; saw 0x00 not 0x01

Is someone have an idea to manage this issue ?

Thanks in advance

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,566 次查看
gfritz
Contributor II

Hi,

Thank you for your answer. We found yesterday the problem : we forgot pull-up on NMI pin (PTA4, pin54 for K10FN1M0xxx12)...

Thank you also for your kind proposition of help

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,566 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you provide the K10 JTAG related circuit?

If yes, we could check the K10 JTAG related schematics.

Customer also could check TWR-K20D50M board schematics about JTAG related circuit design.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,567 次查看
gfritz
Contributor II

Hi,

Thank you for your answer. We found yesterday the problem : we forgot pull-up on NMI pin (PTA4, pin54 for K10FN1M0xxx12)...

Thank you also for your kind proposition of help

0 项奖励
回复