Transmission failed for KEA I2C in Stop mode after waking up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Transmission failed for KEA I2C in Stop mode after waking up

905 次查看
vict
Contributor I

Hi all, 

  When the MCU is waken up from the stop mode through I2C address matching, the first transmission will be lost, i.e. no ACK is received.  Is this by design for KEA?

Regard,

Vic

0 项奖励
回复
1 回复

831 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There is a note about I2C master baud rate requirement during the wake up process:

pastedImage_1.png

The I2C slave need to run the I2C interrupt ISR after wake up the core from the STOP mode, so there need  I2C master add a short delay for I2C to send the ACK signal. 


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复